jr


-

The jr instructions of the device should be specified in the following formats.

-

JR disp22

-

JR disp32

 

-

In asrh, the following formats can also be used in addition to the above.

-

jr22 disp22

-

jr32 disp32

 

-

jr instructions are interpreted as disp22 when the -Xasm_far_jump option is not specified, or disp32 when the -Xasm_far_jump option is specified.

-

jr22 or jr32 should be specified when output should be with a fixed disp width at all times. These instructions will not be affected by the -Xasm_far_jump option.