| 
- | The cmov instruction of the device should be specified in the following formats. | 
| 
- | CMOV    cccc, reg1, reg2, reg3  | 
| 
- | CMOV    cccc, imm5, reg2, reg3 | 
 
| 
- | In asrh, the following formats can also be used in addition to the above. | 
| 
- | cmovcond   reg1, reg2, reg3 | 
| 
- | cmovcond   imm, reg2, reg3 | 
 
Code that can be specified in cond and the result of assembly are the same as those for the setf instruction. For details, see "Table 5.27  setfcond Instruction".
 
| 
- | If the following is specified as imm in syntax "cmov cccc, imm, reg2, reg3" or "cmovcond imm, reg2, reg3", the assembler executes instruction expansion to generate multiple machine instructions. | 
| 
(a) | Absolute expression exceeding the range of -16 to +15, but within the range of -32,768 to +32,767 | 
| cmov    imm4, imm16, reg2, reg3 | movea   imm16, r0, r1 cmov    imm4, r1, reg2, reg3 | 
| 
(b) | Absolute expression having a value exceeding the range of -32,768 to +32,767 | 
If all the lower 16 bits of the value of imm are 0
| cmov    imm4, imm, reg2, reg3 | movhi   HIGHW(imm), r0, r1 cmov    imm4, r1, reg2, reg3 | 
 
Else
| cmov    imm4, imm, reg2, reg3 | mov     imm, r1 cmov    imm4, r1, reg2, reg3 | 
| 
(c) | Relative expression having #label or label, or that having $label for a label having no definition in the sdata/sbss-attribute section | 
| cmov    imm4, #label, reg2, reg3 | mov     #label, r1 cmov    imm4, r1, reg2, reg3 | 
| cmov    imm4, label, reg2, reg3 | mov     label, r1 cmov    imm4, r1, reg2, reg3 | 
| cmov    imm4, $label, reg2, reg3 | mov     $label, r1 cmov    imm4, r1, reg2, reg3 | 
| 
(d) | Relative expression having !label or %label, or that having $label for a label with a definition in the sdata/sbss-attribute section | 
| cmov    imm4, !label, reg2, reg3 | movea   !label, r0, r1 cmov    imm4, r1, reg2, reg3 | 
| cmov    imm4, %label, reg2, reg3 | movea   %label, r0, r1 cmov    imm4, r1, reg2, reg3 | 
| cmov    imm4, $label, reg2, reg3 | movea   $label, r0, r1 cmov    imm4, r1, reg2, reg3 |