20.18 Variable-sized Memory Pool Information (variable_memorypool[])
Here, each variable-sized memory pool is defined.
Parentheses < >show the user input part.
- Description
Define the variable-sized memory pool ID number.
- Definition format
Numeric value
- Definition range
From 1 to 255
- When omitting
The cfg600px assigns the ID number automatically.
- Description
Define the ID name. The specified ID name is output to the system information header file (kernel_id.h) in the form of the following.
#define <ID name> <ID number>
- Definition format
Symbol
- When omitting
Cannot be omitted.
3 ) The size of the variable-sized memory pool (
heap_size)
- Description
Define the size of the variable-sized memory pool area in bytes.
- Definition format
Numeric value
- Definition range
From 24 to 0x10000000
- When omitting
The set value in the default system configuration file (factory setting: 1024) applied.
4 ) Upper limit of the variable-sized memory block (
max_memsize)
- Description
Define the upper limit of an acquirable memory block size in bytes.
- Definition format
Numeric value
- Definition range
From 1 to 0xBFFFFF4
- When omitting
The set value in the default system configuration file (factory setting: 36) applied.
5 ) Section name assigned to the memory pool area (
mpl_section)
- Description
Define the section name to be assigned to the variable-sized memory pool area.
The cfg600px generates the variable-sized memory pool area with the size specified by
heap_size to the section specified by
mpl_section. The section attribute is "DATA", and the alignment number is 4.
When linking, be sure to locate this section in the RAM area. Note, this section must not be located to address 0.
- Definition format
Symbol
- When omitting
The set value in the default system configuration file (factory setting: BRI_HEAP) applied.