20.15 Mutex Information (mutex[])
Here, each mutex is defined.
Parentheses < >show the user input part.
- Description
Define the mutex ID number.
- Definition format
Numeric value
- Definition range
From 1 to 255
- When omitting
The cfg600px assigns the ID number automatically.
- Description
Define the ID name. The specified ID name is output to the system information header file (kernel_id.h) in the form of the following.
#define <ID name> <ID number>
- Definition format
Symbol
- When omitting
Cannot be omitted.
3 ) Ceiling priority (
ceilpri)
- Definition format
Numeric value
- When omitting
The set value in the default system configuration file (factory setting: 1) applied.