Performs processing in response to the external maskable interrupt INTPn.
Remark This API function is called as the interrupt process corresponding to the external maskable interrupt INTPn.
[Syntax]
CA78K0R Compiler
__interrupt static void r_intcn_interrupt ( void );
CC-RL Compiler
static void __near r_intcn_interrupt ( void );
Remark n is the interrupt factor number.
[Argument(s)]
None.
[Return value]
None.