Everything

r_intfo_interrupt

Performs processing in response to the external maskable interrupt INTFO.

Remark         This API function is called as the interrupt process corresponding to the external maskable interrupt INTFO.

 

[Syntax]

CA78K0R Compiler

__interrupt static void   r_intfo_interrupt ( void );

 

CC-RL Compiler

static void   __near r_intfo_interrupt ( void );

 

[Argument(s)]

None.

 

[Return value]

None.