Everything

Usage example

Count the number of falling edge.

 

[GUI setting example]

Interrupt

Used

INTP

Used

INTP0

Valid edge

Falling

Priority

Low

 

[API setting example]

r_main.c

void main(void)

{

       R_MAIN_UserInit();

       /* Start user code. Do not edit comment generated here */

       /* Clear INTP0 interrupt flag and enable interrupt */

       R_INTC0_Start();

 

       while (1U)

       {

              ;

       }

       /* End user code. Do not edit comment generated here */

}

 

r_cg_intc_user.c

/* Start user code for global. Do not edit comment generated here */

volatile uint8_t g_intc0_cnt = 0U;

/* End user code. Do not edit comment generated here */

 

static void __near r_intc0_interrupt(void)

{

       /* Start user code. Do not edit comment generated here */

       /* Count INTP0 */

       g_intc0_cnt++;

       /* End user code. Do not edit comment generated here */

}