Everything

r_intrtcicn_interrupt

Performs processing in response to the external maskable interrupt INTRTCICn.

Remark         This API function is called as the interrupt process corresponding to the external maskable interrupt INTRTCICn.

 

[Syntax]

CA78K0R Compiler

__interrupt static void   r_intrtcicn_interrupt ( void );

 

CC-RL Compiler

static void   __near r_intrtcicn_interrupt ( void );

Remark         n is the interrupt factor number.

 

[Argument(s)]

None.

 

[Return value]

None.