Performs initialization necessary to control the 8-bit interval timer.
Remark This API function is called from R_Systeminit before main() is executed.
[Syntax]
void R_IT8bitm_Channeln_Create ( void );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
None.
[Return value]
None.