Everything

8-bit interval timer

Below is a list of API functions output by the Code Generator for 8-bit interval timer use.

 

Table 3.17 API Functions: [8-Bit Interval Timer]

API Function Name

Function

R_IT8bitm_Channeln_Create

Performs initialization necessary to control the 8-bit interval timer.

R_IT8bitm_Channeln_Create_UserInit

Performs user-defined initialization relating to the 8-bit interval timer.

r_it8bitm_channeln_interrupt

Performs processing in response to the 8-bit interval timer interrupt INTITn0 or INTITn1.

R_IT8bitm_Channeln_Start

Starts the count of the 8-bit interval timer.

R_IT8bitm_Channeln_Stop

Ends the count of the 8-bit interval timer.

R_IT8bitm_Channeln_Set_PowerOff

Halts the clock supplied to the 8-bit interval timer.

R_IT8bitm_Set_PowerOff

Halts the clock supplied to the 8-bit interval timer.