Everything

R_IT8bitm_Channeln_Set_PowerOff

Halts the clock supplied to the 8-bit interval timer.

Remark         Calling this API function changes the 8-bit interval timer to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

 

[Syntax]

void       R_IT8bitm_Channeln_Set_PowerOff ( void );

Remark       m is the unit number, and n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.