Everything

R_IT8bitm_Channeln_Create_UserInit

Performs user-defined initialization relating to the 8-bit interval timer.

Remark         This API function is called as the R_IT8bitm_Channeln_Create callback routine.

 

[Syntax]

void       R_IT8bitm_Channeln_Create_UserInit ( void );

Remark       m is the unit number, and n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.