Performs processing in response to the 8-bit interval timer interrupt INTITn0 or INTITn1.
Remark This API function is called as the interrupt process corresponding to the 8-bit interval timer interrupt INTITn0 or INTITn1.
[Syntax]
CA78K0R Compiler
__interrupt static void r_it8bitm_channeln_interrupt ( void );
CC-RL Compiler
static void __near r_it8bitm_channeln_interrupt ( void );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
None.
[Return value]
None.