Everything

Amplifier unit

Below is a list of API functions output by the Code Generator for Amplifier unit use.

 

Table 3.56   API Functions: [Amplifier unit]

API 関数名

機能概要

R_AMP_Create

Performs initialization necessary to control the amplifier unit.

R_AMP_Create_UserInit

Performs user-defined initialization relatede to the amplifie unit.

R_AMP_Set_PowerOn

Enables amplifier unit power supply.

R_AMP_Set_PowerOff

Disables amplifier unit power supply.

R_PGA1_Start

Starts instrumentation amplifier 1.

R_PGA1_Stop

Stops instrumentation amplifier 1.

R_AMPn_Start

Starts operational amplifier n.

R_AMPn_Stop

Starts operational amplifier n.Stops operational amplifier n.