Parts Buzzer Properties dialog box
|
This property dialog box is used to set or change the pin connection information of a buzzer, which is one of the connection parts in the I/O Panel window.
The pin-connected buzzer displays the information output from the connected pins as a bitmap in the Simulation mode.
The buzzer output can be checked as "display".
There are two types of buzzer display styles, figure and bitmap. These styles can be changed on the [[Style] tab].
Figure A.82 | Parts Buzzer Properties Dialog Box: [Buzzer Connection] Tab |
Figure A.83 | Parts Buzzer Properties Dialog Box: [Style] Tab |
This section describes the following.
[How to open]
On the I/O Panel window, any one of the following:
- | Double-click a part object "Buzzer". |
- | Select [Properties...] form the context menu on a part object "Buzzer". |
- | Select a part object "Buzzer", and then select [Properties...] form the [View] menu. |
[[Buzzer Connection] tab]
(1) | Pin connection information setting area |
Label
|
This area is used to specify the part name. The part name input here is also displayed in the Parts List dialog box as the label.
|
Pin Name
|
This area is used to specify the pin name to be connected (output pin). The connection pins can be specified either via direct input or through selection from the drop-down list.
|
Active Level
|
The active state is selected with a option button, as follows:
|
LOW
|
Sets the active level to LOW.
|
HIGH
|
Sets the active level to HIGH (default).
|
Output Form
|
This item is not allowed to change.
|
Remark | For the pin names that can be specified, see the user's manual of the microcontroller that is used. |
[[Style] tab]
(1) | Style information setting area |
Figure
|
Select this option button to display the buzzer with the following specified figure.
|
Shape
|
Select the figure shape. Two shapes can be selected: rectangle and ellipse.
|
shadow
|
Cannot be selected.
|
Line
|
Specify and change the figure line, as follows.
You can change the color of figure line by clicking the pull-down button.
|
Thickness
|
Specifies the line thickness.
Specification is made either using a spin button or through direct input.
A value from 1 to 100 can be specified.
|
Active
|
Specifies the color of the line during active display.
|
Inactive
|
Specifies the color of the line during inactive display.
|
Fill up
|
Specify and change the figure filling, as follows.
You can change the color of figure filling by clicking the pull-down button.
|
Active
|
Specifies the fill color during active display.
|
Inactive
|
Specifies the fill color during inactive display.
|
Bitmap
|
Select this option button to display the buzzer with the following specified bitmap (default).
|
Selection list
|
Select a bitmap to be used from the selection list.
The selectable bitmaps appear in the selection list.
|
[Add] button
|
Opens the Entry Bitmap dialog box below to add a new bitmap to the selection list.
The bitmap file to be added can be specified either through file selection using the [...] button, or through direct input.
|
[Delete] button
|
Deletes the currently selected bitmap from the selection list.
Note that only the bitmap that have been added by user can be deleted.
|
This area displays the style of the buzzer currently being specified.
[Function buttons]
|
|
OK
|
Validates the settings and closes this dialog box.
|
Cancel
|
Cancels the settings and closes this dialog box.
|
Apply
|
Cannot be selected.
|
Help
|
Displays the help for this dialog box.
|
[Operation]
In the Simulation mode, the active level output of the connected pins can be expressed as a bitmap.
The following bitmaps are displayed according to the pin's output value (active/inactive).
Figure A.84 | Connected Parts Display Example (Buzzer) |