16-bit timer KB
Below is a list of API functions output by the Code Generator for 16-bit timer KB use.
Table 3.10 API Functions: [16-bit Timers KB]
|
API Function Name |
Function |
|
Performs initialization necessary to control the 16-bit timer KB. | |
|
Performs user-defined initialization relating to the 16-bit timer KB. | |
|
Performs processing in response to the timer interrupt. | |
|
Starts the count for 16-bit timer KB. | |
|
Ends the count for 16-bit timer KB. | |
|
Halts the clock supplied to the 16-bit timer KB. | |
|
Enables input of the trigger signal used for the forced output stop function. | |
|
Disables input of the trigger signal used for the forced output stop function. | |
|
Enables batch overwriting of the compare register. | |
|
Enables input of the trigger signal used for the forced output stop function. | |
|
Disables input of the trigger signal used for the forced output stop function. | |
|
Reset the 16-bit timer KB. |