Serial interface UARTMG
Below is a list of API functions output by the Code Generator for serial interface UARTMG use.
Figure 3.55 API Functions: [Serial interface UARTMG]
|
API Function Name |
Function |
|
Performs initialization necessary to control the serial interface UARTMG. | |
|
Performs user-defined initialization related to the serial interface UARTMG. | |
|
Performs processing in response to the UARTMG transmission completion interrupt INTSTMGn. | |
|
Performs processing in response to the UARTMG reception completion interrupt INTSRMGn. | |
|
Perfomrs processing in response to the UARTMG reception error interrupt INTSREMGn. | |
|
Sets UARTMG communication to standby mode. | |
|
Ends UARTMG communication. | |
|
Halts the clock supplied to the serial interface UARTMG. | |
|
Starts UARTMG data transmission. | |
|
Starts UARTMG data reception. | |
|
Performs processing in response to the UARTMG transmission completion interrupt INTSTMGn. | |
|
Performs processing in response to the UARTMG reception completion interrupt INTSRMGn. | |
|
Performs processing in response to the UARTMG reception error interrupt INTSREMGn. | |
|
Performs processing in response to detection of overrun error. |