Comparator
Below is a list of API functions output by the Code Generator for comparator use.
Table 3.28 API Functions: [Comparator]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the comparator.  | |
| 
       Performs user-defined initialization relating to the comparator.  | |
| 
       Performs processing in response to the comparator interrupt INTCMPn.  | |
| 
       Begins comparison of reference input voltage and analog input voltage.  | |
| 
       Stops comparison of reference input voltage and analog input voltage.  | |
| 
       Reset the comparator.  | |
| 
       Halts the clock supplied to the comparator.  |