A/D converter
Below is a list of API functions output by the Code Generator for A/D converter use.
Table 3.22 API Functions: [A/D Converter]
| API Function Name | Function | 
| Performs initialization necessary to control the A/D converter. | |
| Performs user-defined initialization relating to the A/D converter. | |
| Performs processing in response to the A/D conversion end interrupt INTAD. | |
| Enables operation of voltage converter. | |
| Disables operation of voltage converter. | |
| Starts A/D conversion. | |
| Ends A/D conversion. | |
| Reset A/D conversion. | |
| Halts the clock supplied to the A/D converter. | |
| Configures the analog voltage input pin for A/D conversion. | |
| Enables the switch from STOP mode to SNOOZE mode. | |
| Disables the switch from STOP mode to SNOOZE mode. | |
| Sets the operation mode of A/D converter. | |
| Reads the results of A/D conversion (10 bits). | |
| Reads the results of A/D conversion (10 bits). |