Timer RG
Below is a list of API functions output by the Code Generator for timer RG use.
Table 3.8 API Functions: [Timer RG]
|
API Function Name |
Function |
|
Performs initialization necessary to control the 16-bit timer RG0. | |
|
Performs user-defined initialization relating to the 16-bit timer RG0. | |
|
Performs processing in response to the timer interrupt. | |
|
Starts the count for 16-bit timer RG0. | |
|
Ends the count for 16-bit timer RG0. | |
|
Halts the clock supplied to the 16-bit timer RG0. | |
|
Reads the pulse width of the 16-bit timer RG0. |