Common
Below is a list of API functions output by the Code Generator for common use.
Performs processing in response to the exception (other than undefined instruction exception, reset, non-maskable
interrupt and unconditional trap).
Table 3.1 API Functions: [Common]
API Function Name |
Function |
Performs processing in response to the undefined instruction exception. | |
Performs processing in response to the reset. | |
Performs processing in response to the reset. | |
Performs processing in response to the privileged instruction exception. | |
Performs processing in response to the floating-point exception. | |
Performs processing in response to the access exception. | |
Performs processing in response to the non-maskable interrupt. | |
Performs processing in response to the unconditional trap. | |
Performs processing in response to the exception (other than undefined instruction exception, reset, non-maskable interrupt and unconditional trap). | |
Performs initialization necessary to control the various hardwares. | |
Performs initialization necessary to control the various peripheral functions. | |
This is a main function. | |
Performs user-defined initialization. | |
Performs processing in response to the group interrupt. | |
Performs processing in response to the non-maskable interrupt. | |
Performs initialization necessary to control the various hardwares. |