Everything

LCD controller / driver (LCD)

Below is a list of API functions output by the Code Generator for LCD controller / driver use.

 

Table 3.37 API Functions: [LCD controller / driver]

API Function Name

Function

R_LCD_Create

Performs initialization necessary to control the LCD controller / driver.

R_LCD_Create_UserInit

Performs user-defined initialization relating to the LCD controller / driver.

R_LCD_Start

Sets the LCD controller / driver to display on status.

R_LCD_Stop

Sets the LCD controller / driver to display off status.

R_LCD_Voltage_On

Enables operation of internal voltage boost circuit and capacitor split circuit.

R_LCD_Voltage_Off

Disables operation of internal voltage boost circuit and capacitor split circuit.