The following lists the panels/dialog boxes used in the build tool.
Table A.1
List of Panels/Dialog Boxes
Panel/Dialog Box Name
Function Description
Property panel
This panel is used to display the detailed information on the Build tool node or file that is selected on the Project Tree panel and change the settings of the information.
System Include Path Order dialog box
This dialog box is used to refer the system include paths specified for the compiler and set their specified sequence.
Specify Rule Number dialog box
This dialog box is used to select the number of the MISRA-C rule and set it to the area that this dialog box is called from.
Section Settings dialog box
This dialog box is used to add, modify, or delete sections.
Add Section dialog box
Modify Section dialog box
Add Overlay dialog box
These dialog boxes are used to set a section name when adding, modifying, or overlaying a section, respectively.
Section Address dialog box
This dialog box is used to set an address when adding or modifying a section.
Unassigned Section dialog box
This dialog box is used to delete sections.
CRC Operations dialog box
This dialog box is used to add, modify, or delete the CRC operation settings.
Select Modules Which Are Output in Files dialog box
This dialog box is used to set modules which are output to the I/O header file.
Select Constituent Application Projects dialog box
This dialog box is used to set the constituent application projects.