Everything
19.4 System Information (system)
Here, information on the system whole is defined.
Only one "system" can be defined. And the "system" can not be omitted.
Format
Parentheses < >show the user input part.
1 ) System stack size (stack_size)
- Description
Define the total stack size used in service call processing and interrupt processing.
- Definition format
Numeric value
- Definition range
More than 8, and multiple of 4.
- When omitting
The set value in the default system configuration file (factory setting: 0x800) applied.
2 ) Maximum task priority (priority)
- Description
Define the maximum task priority.
- Definition format
Numeric value
- Definition range
1 - 255
- When omitting
The set value in the default system configuration file (factory setting: 32) applied.
- TMAX_TPRI
The cfg600 outputs the macro TMAX_TPRI which defines this setting to the system information header file "kernel_id.h".
3 ) Kernel interrupt mask level (system_IPL)
- Description
Define the interrupt mask level when the kernel's critical section is executed (PSW register's IPL value). Interrupts with higher priority levels than that are handled as "non-kernel interrupts".
For details of "non-kernel interrupts" and "kernel interrupts", refer to "10.1 Interrupt Type".
- Definition format
Numeric value
- Definition range
1 - 15
- When omitting
The set value in the default system configuration file (factory setting: 7) applied.
- VTKNL_LVL
The cfg600 outputs the macro VTKNL_LVL which defines this setting to the system information header file "kernel_id.h".
4 ) Maximum message priority (message_pri)
- Description
Define the maximum message priority used in the mailbox function. Note that if the mailbox function is not used, this definition item has no effect.
- Definition format
Numeric value
- Definition range
1 - 255
- When omitting
The set value in the default system configuration file (factory setting: 255) applied.
- TMAX_MPRI
The cfg600 outputs the macro TMAX_MPRI which defines this setting to the system information header file "kernel_id.h".
5 ) Denominator of base clock interval time (tic_deno)
- Description
The base clock interval time is calculated by the following expression. Either tic_deno or tic_nume should be 1.
The base clock interval time (in millisecond) = tic_nume / tic_deno
- Definition format
Numeric value
- Definition range
1 - 100
- When omitting
The set value in the default system configuration file (factory setting: 1) applied.
- TIC_DENO
The cfg600 outputs the macro TIC_DENO which defines this setting to the system information header file "kernel_id.h".
6 ) Numerator of base clock interval time (tic_nume)
- Description
See above.
- Definition format
Numeric value
- Definition range
1 - 65535
- When omitting
The set value in the default system configuration file (factory setting: 1) applied.
- TIC_NUME
The cfg600 outputs the macro TIC_NUME which defines this setting to the system information header file "kernel_id.h".
7 ) Task context register (context)
- Description
Define the register set used by tasks. The settings made here apply to all tasks.
- Definition format
Symbol
- Definition range
Select one from item of "Setting" in Table 19-2.
Table 19-2 system.context
Setting
CPU
FPU
DSP
PSW, PC, R0 - R7, R14, R15
R8 - R13
FPSW
Accumulator 1
NO
Guaranteed
Guaranteed
Not guaranteed
Not guaranteed
FPSW
Guaranteed
Guaranteed
Guaranteed
Not guaranteed
ACC
Guaranteed
Guaranteed
Not guaranteed
Guaranteed
FPSW,ACC
Guaranteed
Guaranteed
Guaranteed
Guaranteed
MIN
Guaranteed
Not guaranteed
Not guaranteed
Not guaranteed
MIN,FPSW
Guaranteed
Not guaranteed
Guaranteed
Not guaranteed
MIN,ACC
Guaranteed
Not guaranteed
Not guaranteed
Guaranteed
MON,FPSW,ACC
Guaranteed
Not guaranteed
Guaranteed
Guaranteed
1
When compiler option "-isa=rxv2" is specified, the "Accumulator" means ACC0 register and ACC1 register. In the case of others, the "Accumulator" means ACC0 register (in RXv2 architecture) or ACC register (in RXV1 architecture).


Note Compiler option -isa is supported by the compiler CC-RX V2.01 or later.
- When omitting
The set value in the default system configuration file (factory setting: NO) applied.
- Note
Be sure to refer to "19.5 Note Concerning system.context".