Everything
19.17 Alarm Handler Information (alarm_handl[])
Here, each alarm handler is defined.
Format
Parentheses < >show the user input part.
 alarm_hand[ <1. ID number> ] {
     name           = <2. ID name (name)>;
     entry_address  = <3. Alarm handler entry address (entry_address)>;
     exinf          = <4. Extended information (exinf)>;
 };

1 ) ID number
- Description
Define the alarm handler ID number.
- Definition format
Numeric value
- Definition range
From 1 to 255
- When omitting
The cfg600 assigns the ID number automatically.
- Note
The ID numbers must be assigned without an omission beginning with 1. Therefore, when specifying an ID number, be sure that the specified value is equal to or less than the number of objects defined.
2 ) ID name (name)
- Description
Define the ID name. The specified ID name is output to the system information header file (kernel_id.h) in the form of the following.
 #define   <ID name>   <ID number>
- Definition format
Symbol
- Definition range
-
- When omitting
Cannot be omitted.
3 ) Alarm handler entry address (entry_address)
- Description
Define the starting function of the alarm handler.
- Definition format
Symbol
- Definition range
-
- When omitting
Cannot be omitted.
4 ) Extended information (exinf)
- Description
Define the extended information of the alarm handler.
- Definition format
Numeric value
- Definition range
From 0 to 0xFFFFFFFF
- When omitting
The set value in the default system configuration file (factory setting: 0) applied.
- Note
The extended information is passed to the alarm handler.