Everything
 

Encoding dialog box


This dialog box is used to select a file-encoding.

Figure A.6

Encoding Dialog Box

 

This section describes the following.

[How to open]

-

From the [File] menu, open the Open File dialog box by selecting [Open with Encoding...], and then click the [Open] button in the dialog box.

[Description of each area]

(1)

[Available encodings]

Select the encoding to be set.

The encoding of the selected file is selected by default.

[Function buttons]

Button

Function

OK

Opens the selected file in the Open File dialog box using a selected file encoding.

Cancel

Not open the selected file in the Open File dialog box and closes this dialog box.

Help

Displays the help for this dialog box.