| 
 Find and Replace dialog box 
 | 
This dialog box is used to find and replace the designated characters.
Figure A.8  | Find and Replace Dialog Box  | 
 
Remark  | The  
 button in [Search text] will be displayed only if this dialog box is opened from the Editor panel.  | 
 
 
The following items are explained here.
[How to open]
-  | From the [Edit] menu, select [Find...].  | 
 
-  | From the [Edit] menu, select [Replace...].  | 
 
-  | [Ctrl] + [F] key, [Ctrl] + [R] key, [Ctrl] + [Shift] + [F] key or [Ctrl] + [Shift] + [R] key.  | 
 
[Description of each area]
Find/replace is switched when a tab is selected.
This dialog box has the following tabs.
(2)  | Search/replace criteria setting area  | 
 
Detailed criteria for searching/replacing is set.
Please see the description of the relevant tabs for details of the contents/how to set.
[Function buttons]
Buttons for execute find/replace.
Please see the description of the relevant buttons for details.