Windows/panels/dialog boxes used with the editor features are listed below.
Table A.1
Window/Panel/Dialog Box List
Window/Panel/Dialog Box Name
Description
Editor panel
Enables text files to be viewed and edited, and is used to execute source level debug.
Encoding dialog box
Selects a file-encoding.
Save Settings dialog box
Specifies the encoding and the new line code of the file being edited.
Find and Replace dialog box
Finds and replaces the designated characters.
Go to Line dialog box
Moves the caret to the specified line.
Jump to Function dialog box
Selects a function to which the caret moves.
Bookmarks dialog box
Displays and deletes bookmarks.
Print Preview window
Previews the source file before printing.