Below is a list of CS+ Python functions (for the build tool).
Table B.4
CS+ Python Function (For build Tool)
Function Name
Function Description
build.All
This function runs a build.
build.ChangeBuildMode
This function changes the build mode.
build.Clean
This function runs a clean.
build.File
This function runs a build of a specified file.
build.Stop
This function stops the currently running build.
build.Update
This function updates the dependencies for the build tool.