Everything
B.3.7 CS+ Python property (common)

Below is a list of CS+ Python properties (common).

Table B.7

CS+ Python Property (Common)

Property Name

Function Description

common.ExecutePath

This property refers to the absolute path of the folder containing the exe file of the currently running CS+.

common.ConsoleClear

This property sets or refers to whether to clear the display of the Python console when changing the active project.

common.EnableRemotingStartup

This property sets and displays the setting for enabling or disabling the function for linking to an external tool at CS+ startup.

common.Output

This property refers to the return value or the contents of an error of the CS+ Python function.

common.ThrowExcept

This property sets or refers to whether to throw an exception during the Python function is executed.

common.UseRemoting

This property sets and displays the setting for enabling or disabling the function for linking to an external tool at CS+ startup.

common.Version

This property refers to the version of CS+.

common.ViewLine

This property sets or refers to the number of screen lines for the Python console.

common.ViewOutput

This property sets and displays the setting for whether or not to display results of Python functions for CS+ and error messages in the Python console.