Everything
B.3.2 CS+ Python function (common)

Below is a list of CS+ Python functions (common).

Table B.2

CS+ Python Function (Common)

Function Name

Function Description

common.GetOutputPanel

This function displays the contents of the Output panel.

common.OutputPanel

This function displays the string on the Output panel.

common.PythonInitialize

This function initializes Python.

server.Start

Start socket communication to connect with Python 3 execution environment.

server.Stop

Stop socket communication to connect with Python 3 execution environment.