Everything

build.Compile.AdditionalOptions


This property sets or refers to the compile options for the active project regarding other additional options.

[Specification format]

build.Compile.AdditionalOptions = option

[Setting(s)]

Setting

Description

option

Set the additional compile options as strings.

[Reference]

Additional compile options (strings)

[Detailed description]

-

This property sets or refers to the compile options for the active project regarding other additional options.

-

The options set here are added at the end of the compile options group.

[Example of use]

>>>build.Compile.AdditionalOptions = "-o3 -Xvolatile"   ... Set multiple options
>>>print build.Compile.AdditionalOptions
-o3 -Xvolatile
>>>copt = build.Compile.AdditionalOptions + " -v"   ... Refer the current setting and add an option
>>>build.Compile.AdditionalOptions = copt
>>>print build.Compile.AdditionalOptions
-o3 -Xvolatile -v
>>>