This property is for setting or referring to the range of a debug monitoring area. It is a link option for the active project. [CC-RL]
Range of a debug monitoring area
This property is for setting or referring to the range of a debug monitoring area. It is a link option for the active project. |
This property can only be set or referred to when [Set debug monitor area] (build.Link.SetDebugMonitorArea) has been specified for [Yes(Specify address range)] (DebugMonitorArea.SpecifiedAddressRange). |