This property is for setting or referring to whether or not mathf.h (C89/C99) is enabled. It is a library generate option for the active project. [CC-RX]
Set whether or not mathf.h (C89/C99) is enabled. |
When mathf.h (C89/C99) and the runtime library are enabled: True
When mathf.h (C89/C99) is disabled: False
This property is for setting or referring to whether or not mathf.h (C89/C99) is enabled. It is a library generate option for the active project. |