build.HexOutput.OutputFolder
|
This property is for setting or referring to the folder for hexadecimal output. It is a hexadecimal output option for the active project.
[Specification format]
build.HexOutput.OutputFolder = folder
|
[Setting(s)]
|
|
folder
|
Set the path to the folder for hexadecimal output as strings.
|
[Reference]
Path to the folder for hexadecimal output
[Detailed description]
- | This property is for setting or referring to the folder for hexadecimal output. It is a hexadecimal output option for the active project. |
[Example of use]
>>>build.HexOutput.OutputFolder = "/ProjectDir/Output_Vx.xx.xx"
>>>print build.HexOutput.OutputFolder
%ProjectDir%\Output_Vx.xx.xx
>>>
|