Everything

build.Link.SectionSymbolFile


This property sets or refers to the link options for the active project regarding sections whose external defined symbols are to be output to a file. [CC-RH][CC-RX][CC-RL]

[Specification format]

build.Link.SectionSymbolFile = sectionlist

[Setting(s)]

Setting

Description

sectionlist

Set the section whose external defined symbols are output to a file as a list of strings.

[Reference]

List of the section whose external defined symbols are output to a file

[Detailed description]

-

This property sets or refers to the link options for the active project regarding sections whose external defined symbols are to be output to a file.

-

Add or change for the referred list to change the setting.

[Example of use]

>>>sec = build.Link.SectionSymbolFile   ... Refer the current setting and add the section whose external defined symbols are output to a file
>>>print sec
['R_1', 'R_2']
>>>sec.append('R_3')
>>>build.Link.SectionSymbolFile = sec
>>>print build.Link.SectionSymbolFile
['R_1', 'R_2', 'R_3']