24-bit DS A/D converter
Below is a list of API functions output by the Code Generator for 24-bit ΔΣ A/D converter use.
Table 3.25 API Functions: [224-bit ΔΣ A/D Converter]
| API Function Name | Function | 
| Performs initialization necessary to control the 24-bit ΔΣ A/D converter. | |
| Performs user-defined initialization relating to the 24-bit ΔΣ A/D converter. | |
| Performs processing in response to the ΔΣ A/D conversion end interrupt INTDSAD. | |
| Performs processing in response to the zero-cross detection interrupt INTDSADZCn. | |
| Enables operation of 24-bit ΔΣ A/D converter. | |
| Disables operation of 24-bit ΔΣ A/D converter. | |
| Starts A/D conversion. | |
| Ends A/D conversion. | |
| Reset the 24-bit ΔΣ A/D converter. | |
| Performs electric charge reset for the 24-bit ΔΣ A/D converter. | |
| Reads the results of A/D conversion (24 bits). | |
| Reads the results of A/D conversion (16 bits; most significant 16 bits of 24-bit resolution). |