Asynchronous serial interface LIN-UART
Below is a list of API functions output by the Code Generator for asynchronous serial interface LIN-UART (UARTF) use.
Table 3.33 API Functions: [Asynchronous Serial Interface LIN-UART]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the asynchronous serial interface LIN-UART (UARTF).  | |
| 
       Performs user-defined initialization related to the asynchronous serial interface LIN-UART (UARTF).  | |
| 
       Performs processing in response to the LIN-UART transmission end interrupt INTLT.  | |
| 
       Performs processing in response to the LIN-UART reception end interrupt INTLR.  | |
| 
       Performs processing in response to the LIN-UART reception status interrupt INTLS.  | |
| 
       Sets LIN communication to standby mode.  | |
| 
       Ends LIN communication.  | |
| 
       Halts the clock supplied to the asynchronous serial interface LIN-UART (UARTF).  | |
| 
       Starts UARTF data transmission.  | |
| 
       Starts UARTF data reception.  | |
| 
       Starts the data comparison.  | |
| 
       Ends the data comparison.  | |
| 
       Performs processing in response to the LIN-UART transmission end interrupt INTLT.  | |
| 
       Performs processing in response to the LIN-UART reception end interrupt INTLR.  | |
| 
       Performs processing in response to the LIN-UART reception status interrupt INTLS.  | |
| 
       Performs processing in response to detection of overrun error.  | |
| 
       Performs processing in response to detection of expansion bit.  | |
| 
       Performs processing in response to match of ID parity.  |