External signal sampler
Below is a list of API functions output by the Code Generator for External signal sampler use.
Table 3.54 API Functions: [External signal sampler]
| API Function Name | FUnction | 
| Performs initialization necessary to control the External signal sampler. | |
| Performs user-defined initialization relating to the External signal sampler. | |
| Performs processing in response to the External signal sampler edge detection interrupt INTEXSD. | |
| Starts External signal sampling. | |
| Ends External signal sampling. | |
| Halts the clock supplied to the External signal sampler. |