Clock output/buzzer output controller
Below is a list of API functions output by the Code Generator for clock output/buzzer output controller use.
Table 3.19 API Functions: [Clock Output/Buzzer Output Controller]
| API Function Name | Function | 
| Performs initialization necessary to control the clock/buzzer output controller. | |
| Performs user-defined initialization relating to the clock/buzzer output controller. | |
| Starts clock/buzzer output. | |
| Ends clock/buzzer output. | |
| Halts the clock supplied to the clock/buzzer output controller. |