16-bit timer KB2
Below is a list of API functions output by the Code Generator for 16-bit timer KB2 use.
Table 3.12 API Functions: [16-bit Timer KB2]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the 16-bit timer KB2.  | |
| 
       Performs user-defined initialization relating to the 16-bit timer KB2.  | |
| 
       Performs processing in response to the timer interrupt INTTKB2m.  | |
| 
       Starts the count for 16-bit timer KB2.  | |
| 
       Ends the count for 16-bit timer KB2.  | |
| 
       Halts the clock supplied to the 16-bit timer KB2.  | |
| 
       Starts the simultaneous start/stop mode.  | |
| 
       Ends the simultaneous start/stop mode.  | |
| 
       Starts the timer start/clear mode.  | |
| 
       Ends the timer start/clear mode.  | |
| 
       Starts forced output stop function 1 for timer output TKBOn0.  | |
| 
       Ends forced output stop function 1 for timer output TKBOn0.  | |
| 
       Starts forced output stop function 2 for timer output TKBOn1.  | |
| 
       Starts forced output stop function 2 for timer output TKBOn1.  | |
| 
       Starts dithering function for timer output TKBOn0.  | |
| 
       Ends dithering function for timer output TKBOn0.  | |
| 
       Starts dithering function for timer output TKBOn1.  | |
| 
       Ends dithering function for timer output TKBOn1.  | |
| 
       Starts smooth start function for timer output TKBOn0.  | |
| 
       Ends smooth start function for timer output TKBOn0.  | |
| 
       Starts smooth start function for timer output TKBOn1.  | |
| 
       Ends smooth start function for timer output TKBOn1.  | |
| 
       Enables batch overwriting of the compare register.  |