< Compile Options / Microcontroller Options >
The default for this option is denormalize=off.
This option specifies the operation when denormalized numbers are used to describe floating-point constants.  | 
This option does not affect the handling of denormalized numbers in floating-point operations during program execution.  |