< Compile Options / Microcontroller Options >
[Format]
[Description]
-  | This option is used to avoid a problem specific to the CPU type.  | 
 
-  | When -patch=rx610 is specified, the MVTIPL instruction which causes a problem in the RX610 Group is not used in the generated code. Unless -patch=rx610 is specified, the code generated in response to the call by the intrinsic function set_ipl will contain the MVTIPL instruction.  |