< Compile Options / Microcontroller Options >
[Format]
 
The C++ exceptional handling function (try, catch, throw) is disabled.
[Description]
-  | The C++ exceptional handling function (try, catch, throw) is enabled.  | 
 
-  | The code performance may be lowered.  | 
 
[Remarks]
-  | In order to use the C++ exceptional handling function among files, perform the following:  | 
 
-  | Do not specify the noprelink option in the optimizing linkage editor.  | 
 
-  | The exception option can be specified only at C++ compilation. The exception option is ignored when lang=cpp has not been specified and the input file extension is .c or .p.  |