< Compile Options / Microcontroller Options >
The default for this option is unpack. That is, the structure members and class members have boundary alignment values appropriate for their types. The boundary alignment value for structures and classes equals the maximum boundary alignment value for members.
The structure members and class members have boundary alignment values appropriate for their types.  | 
The boundary alignment value for structures and classes equals the maximum boundary alignment value for members.  | 
The boundary alignment values for structure members and class members when these options are specified are shown in the following table.  | 
Boundary Alignment Values for Structure Members and Class Members When the unpack Option is Specified  |