|
debugger.Assemble.LineAssemble
|
This function performs line assembly.
[Specification format]
debugger.Assemble.LineAssemble(address, code)
|
[Argument(s)]
|
|
|
|
address
|
Specify the address at which to start assembly.
|
|
code
|
Specify the string to assemble.
|
[Return value]
If line assembly was performed successfully: True
If there was an error when performing line assembly: False
[Detailed description]
- | This function performs assembly of the string specified by code from the address specified by address. |
- | If "." is specified in address, then it is interpreted as the address following the last address assembled. |
[Example of use]
>>>debugger.Assemble.Disassemble("main")
0x00004088 F545 br _TestInit+0x8e
>>>debugger.Assemble.Disassemble(".")
0x0000408A 0A5A mov 0xa, r11
>>>debugger.Assemble.LineAssemble("main", "mov r13, r12")
True
>>>debugger.Assemble.Disassemble("main", 1, False)
0x00004088 mov r13, r12
>>>
|