This function fills the memory.
[Specification format]
debugger.Memory.Fill(address1, address2, value, memoryOption = MemoryOption.Byte)
|
[Argument(s)]
|
|
|
|
address1
|
Specify the start address to fill.
|
|
address2
|
Specify the end address to fill to.
|
|
value
|
Specify the fill value.
|
|
memoryOption
|
Specify the fill unit.
The units that can be specified are shown below.
|
|
|
|
|
MemoryOption.Byte
|
Byte unit (8 bits) (default)
|
|
MemoryOption.HalfWord
|
Half-word unit (16 bits) [RH850,RX,V850]
|
|
MemoryOption.Word
|
Word unit (RL78,78K: 16 bits, RH850,RX,V850: 32 bits)
|
[Return value]
If the memory was filled successfully: True
If there was an error when filling the memory: False
[Detailed description]
- | This function fills from address1 to address2 with value. |
- | If memoryOption is specified, fill according to that specification. |
[Example of use]
>>>debugger.Memory.Fill(0x1000, 0x2000, 0xFF)
True
>>>debugger.Memory.Fill(0x2000, 0x3000, 0x0A, MemoryOption.Word)
False
>>>
|