|
debugger.Interrupt.PseudoInterrupt
|
This function generates pseudo-interrupts. [RL78 instruction simulator]
[Specification format]
debugger.Interrupt.PseudoInterrupt(vectorAddress, priority)
|
[Argument(s)]
|
|
|
|
vectorAddress
|
Specify the interrupt name (string) or vector address (numerical value: 0x4 to 0x7c).
|
|
priority
|
Specify the interrupt priority (numerical value: 0 to 3).
|
[Return value]
If interrupts were generated successfully : True
If there was an error when generating interrupts : False
[Detailed description]
- | An interrupt is generated in the interrupt enable (EI) state. |
- | An interrupt is reserved in the interrupt disable (DI) state and generated when the state next becomes interrupt enable (EI). |
- | Setting registers for the interrupt functions is not required. Among such registers, only the PSW is changed by an interrupt. |
- | If a reset is generated while an interrupt is held pending, this interrupt will be deleted. |
[Example of use]
>>>debugger.Interrupt.PseudoInterrupt(8, 0)
True
>>>debugger.Interrupt.PseudoInterrupt("INTWDTI", 1)
True
>>>
|