|
|
|
|
feVectorType
|
Specify the type of an interrupt.
The types that can be specified are shown below.
|
|
|
|
|
FEVectorType.FENMI
|
NMI interrupt [RH850G3M, RH850G3K, RH850G3MH, RH850G3KH, RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT
|
INT interrupt [RH850G3M, RH850G3K, RH850G3MH, RH850G3KH]
|
|
FEVectorType.FEINT0
|
INT interrupt 0 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT1
|
INT interrupt 1 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT2
|
INT interrupt 2 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT3
|
INT interrupt 3 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT4
|
INT interrupt 4 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT5
|
INT interrupt 5 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT6
|
INT interrupt 6 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT7
|
INT interrupt 7 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT8
|
INT interrupt 8 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT9
|
INT interrupt 9 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT10
|
INT interrupt 10 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT11
|
INT interrupt 11 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT12
|
INT interrupt 12 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT13
|
INT interrupt 13 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT14
|
INT interrupt 14 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.FEINT15
|
INT interrupt 15 [RH850G4MH (versions earlier than 2.0)]
|
|
FEVectorType.SyserrCause10
|
SyserrCause10 interrupt
|
|
FEVectorType.SyserrCause11
|
SyserrCause11 interrupt
|
|
FEVectorType.SyserrCause12
|
SyserrCause12 interrupt
|
|
FEVectorType.SyserrCause13
|
SyserrCause13 interrupt
|
|
FEVectorType.SyserrCause14
|
SyserrCause14 interrupt
|
|
FEVectorType.SyserrCause15
|
SyserrCause15 interrupt
|
|
FEVectorType.SyserrCause16
|
SyserrCause16 interrupt
|
|
FEVectorType.SyserrCause17
|
SyserrCause17 interrupt
|
|
FEVectorType.SyserrCause18
|
SyserrCause18 interrupt
|
|
FEVectorType.SyserrCause19
|
SyserrCause19 interrupt
|
|
FEVectorType.SyserrCause1a
|
SyserrCause1a interrupt
|
|
FEVectorType.SyserrCause1b
|
SyserrCause1b interrupt
|
|
FEVectorType.SyserrCause1c
|
SyserrCause1c interrupt
|
|
FEVectorType.SyserrCause1d
|
SyserrCause1d interrupt
|
|
FEVectorType.SyserrCause1e
|
SyserrCause1e interrupt
|
|
FEVectorType.SyserrCause1f
|
SyserrCause1f interrupt
|
|
isGuestMode
|
Specifies whether the device context that raises the exception is in guest mode.
True : Guest mode
False : Host mode or conventional mode (default)
|
|
gpid
|
Specify the GPID of the device context that causes the exception.
None :: Do not specify GPID (default)
(numeric value) : GPID of the device context that raises the exception.
|