16-bit timer KB2
Below is a list of API functions output by the Code Generator for 16-bit timer KB2 use.
Table 3.12 API Functions: [16-bit Timer KB2]
|
API Function Name |
Function |
|
Performs initialization necessary to control the 16-bit timer KB2. | |
|
Performs user-defined initialization relating to the 16-bit timer KB2. | |
|
Performs processing in response to the timer interrupt INTTKB2m. | |
|
Starts the count for 16-bit timer KB2. | |
|
Ends the count for 16-bit timer KB2. | |
|
Halts the clock supplied to the 16-bit timer KB2. | |
|
Starts the simultaneous start/stop mode. | |
|
Ends the simultaneous start/stop mode. | |
|
Starts the timer start/clear mode. | |
|
Ends the timer start/clear mode. | |
|
Starts forced output stop function 1 for timer output TKBOn0. | |
|
Ends forced output stop function 1 for timer output TKBOn0. | |
|
Starts forced output stop function 2 for timer output TKBOn1. | |
|
Starts forced output stop function 2 for timer output TKBOn1. | |
|
Starts dithering function for timer output TKBOn0. | |
|
Ends dithering function for timer output TKBOn0. | |
|
Starts dithering function for timer output TKBOn1. | |
|
Ends dithering function for timer output TKBOn1. | |
|
Starts smooth start function for timer output TKBOn0. | |
|
Ends smooth start function for timer output TKBOn0. | |
|
Starts smooth start function for timer output TKBOn1. | |
|
Ends smooth start function for timer output TKBOn1. | |
|
Enables batch overwriting of the compare register. |